Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the projection of the HVL switch operating handle in the closed (up) position?
Issue:
HVL switch operating handle projection

Product Line:
Switchboards and Switchgear

Environment:
Medium Voltage Switchgear

Resolution:
The handle for the Over Toggle Mechanism (OTM) projects out 4.0`` in the closed position.
The handle for the Stored Energy Mechanism (SEM) projects out 5.0`` in the closed position.