Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Does SquareD/Schneider Electric provide lugs, either mechanical or compression, as a standard feature on Low Voltage Dry Type Distribution Ventilated Transformers?
Issue:
Transformer Lugs

Product Line:
LV Transformers

Environment:
Applies to Ventilated and Non Ventilated Transformers by SquareD/Schneider Electric

Cause:
Lugs are required on Ventilated and Non Ventilated Transformers


Resolution:
Due to the complexity of a Transformer`s possible installation due to specific application variables, SquareD/Schneider Electric does not include lugs with the Transformer.  It is much more beneficial for the installer to select the lugs most appropriate for the specifics of the individual Transformer`s installation.  As well, the specifying engineer may have specific requirements.  However, as a convenience, SquareD/Schneider Electric does offer a range of mechanical and compression lug kits.  The kVA range is listed for the kits as a guide only.  The contents of each kit is clearly spelled out so the customer can select the kit most appropriate for his installation`s requirements.


CTA-ID : 2034172