Issue:
Branch breakers size to be installed in an NF panel with a 400A main breaker.
Product Line:
Panelboards
Environment:
NF
Cause:
Selection
Resolution:
The standard branch breakers go to 125A in 2 & 3 pole configuration.
For NF panels with a LA/LH main breaker, up to two 250a J Frame sub feed breakers can be mounted with the proper size back box and trim.
Sub-feed circuit breakers CANNOT be be field installed onto NF Panelboards with PowerPacT L main circuit breakers
Publicado para: Schneider Electric Mexico