Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Do we have a busway offering with a 200% rated neutral?
Issue:
Busway  with 200% rated neutral.

Product Line:
I-Line Busway

Environment:
Products sold in North America

Resolution:
No. The amperage of the busway will need to be double the anticipate load. ( i.e. for a 600A load, a 1200A busway will need to be ordered)