Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
On a factory assembled NQ panel with a weatherproof MH*WP box, can the factory punch an opening in it to accommodate a specific hub?
Issue:
Can the factory punch an opening in a factory assembled NQ panel with a weatherproof box to accommodate a 3.5`` hub?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosure systems sold and supported in the USA.

Cause:
Can the factory install a conduit opening in an MH*WP panelboard backbox to customer specifications?

Resolution:
On the MH/WP enclosures, the endwalls are shipped blank. The factory is unable to punch holes for the customer, as doing so would void the UL listing on the enclosure as it leaves the factory.