Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Can a Model 5 MCC Bucket be placed in new Model 6 MCC section
Issue:
Model 5 MCC Bucket can be placed in new Model 6 MCC section

Product Line:
Motor Control Centers

Environment:
Maintenance / Installation

Cause:
Clarification

Resolution:
The Model 5 bucket will be able to mount into a new Rev 05 ( Oct 2005 and Later) Mdl 6 MCC structure.
The midshelf that comes in the new Model 6 MCC section will need to have the pin drilled out in order for the butterfly on the Model 5 bucket to latch into the Model 6 MCC section.