Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What gauge of steel is used for the enclosure of a 3T2F Transformer?
Issue:
Steel gauge on Epoxy Resin Encapsulated Transformers

Product Line:
LV Transformers

Environment:
Applies to Epoxy Resin Encapsulated Transformers by SquareD/Schneider Electric

Cause:
ERET Transformer enclosures are made of steel

Resolution:
The main enclosure is made of 16 gauge steel. The mounting flanges are made of 10 gauge steel.


CTA-ID : 2046470