Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Is there a replacement for the obsolete QM1BL, QM3BL, QW1BL and QW3BL filler blanks, for the QM and QW series 1 -4, and series D2 QMB panels?
Issue:
Replacement for obsolete filler blanks for the QM and QW series 1 -4, and series D2 QMB panels

Product Line:
Panelboards.

Environment:
QMB, QM, and QW series 1 - 4 and D2 panels

Cause:
Product features.

Resolution:
These are obsolete with no replacement.
Suggest installer to have fabrication done at a local sheet metal shop.