Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the torque value for a 42 circuit 400 amp NQ Main lug panel`s main lugs?
Issue:
Torque value for a 42 circuit 400 amp NQ Main lug panel

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Maintenance.

Resolution:
Lug can accept (1) 1/0-750 kcmil conductor, or (2) 1/0-350 kcmil which needs to be torqued to 275-300 in lbs.


CTA-ID : 2047831