Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Are there alternate lugs for an NQ 400 amp MLO panel that will accommodate 2 sets of 400-750 kcmil per phase?
Issue:
Optional lug for a 400 amp MLO NQ panel accepting (2) 400-750 kcmil per phase

Product Line:
NQ Panelboards

Environment:
Application

Resolution:
A 600A lug kit, catalog number NQALM6, will accomodate (2) 1/0-750 kcmil per phase and can be used in a 400A MLO panel