Issue:
Determining the Optimal Installation Location of SDSA1175/SDSA1175T Surge Protective Devices Within the Electrical Panel
Product Line:
Surge Protection.
Environment:
Products sold in the United States.
Cause:
Assembly, Installation.
Resolution:
To optimize the performance of the SDSA1175/SDSA1175T surge protective device (SPD), conductors should be twisted and kept as short as possible by trimming excess wire. Avoid looping, coiling, or introducing sharp bends in the conductors, as these can increase impedance and reduce surge suppression effectiveness. The SPD should be connected to the circuit breaker(s) located in closest proximity to minimize lead length. Extended conductor lengths can significantly degrade the device’s clamping response and overall performance.
Publicado para: Schneider Electric Mexico