Issue:
NQ panelboard NQXXRDE Rail extension kit and the NF panelboard NFXXRDE extension kit to be used in both NEMA 1 and NEMA 3R enclosures
Product Line:
NQ/NF Panelboards
Environment:
Application
Cause:
Clarification
Resolution:
Yes. Both Rail extension kits can be used in both indoor MH** NEMA 1 and outdoor MH**WP NEMA 3R type enclosures. These are used to extend the interior in order for it to fit it into a larger enclosure.
Note : This is NOT a Box extension kit used to increase the length of the enclosure.
NQ panelboard NQXXRDE Rail extension kit and the NF panelboard NFXXRDE extension kit to be used in both NEMA 1 and NEMA 3R enclosures
Product Line:
NQ/NF Panelboards
Environment:
Application
Cause:
Clarification
Resolution:
Yes. Both Rail extension kits can be used in both indoor MH** NEMA 1 and outdoor MH**WP NEMA 3R type enclosures. These are used to extend the interior in order for it to fit it into a larger enclosure.
Note : This is NOT a Box extension kit used to increase the length of the enclosure.
Publicado para: Schneider Electric Mexico