Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the content of catalog number 8011306801, pertaining to NF panelboards?
Issue:
Content of Part Number 8011306801

Product Line:
Panelboards.

Environment:
Products sold and used in North America

Cause:
Product features.

Resolution:
This is a Square D internal part number for an NF panelboard blank filler plate for a single pole EDB, EGB, or EJB type breaker.
Order catalog number NFFP15, which is a package of 15 of them.