Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Will an NQ430L1 mount in an MH38WP box?

Issue:
Will an NQ430L1 / NQ430L1C, that normally mounts in an MH32WP box, mount in an MH38WP box?

Product Line:
NQ RTI Panelboard

Environment:
NEMA3R enclosure

Cause:
The NQ430L1 / NQ430L1C is used with an MH32WP but customer wants to use an MH38WP which he has in stock. Are there going to be any mounting issues.

Resolution:
Yes, use the NQ6RDE, 6 inch rail extension kit with the NQ430L1 / NQ430L1C and this will allow the interior to be mounted in the MH38WP enclosure.