Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Are NQ and NF Panel Nema 1 and Nema 3R enclosures welded at the seams?

Issue:
Are NQ and NF Panel Nema 1 and Nema 3R enclosures welded at the seams?

Product Line:
NQ/NF Panelboards

Environment:
Design and Construction standard

Cause:
Clarification

Resolution:
The Nema 1 and Nema 3R enclosures are no longer provided with Welded seams, they are bolted together with the Nema 3R enclosure getting sealed with Silicone for water tightness.