Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Are all NEMA 3R covers for Speed-D and QED switchboards hinged on the same side?
Issue:
Product Features

Product Line:
QED switchboards

Environment:
NEMA PB-2, UL 891, NFPA 70 Art. 408

Cause:
An understanding of this feature can help identify replacement parts, when needed.

Resolution:
A detailed explanation is required:
  • Speed-D NEMA 3R enclosure doors are hinged opposite of QED-2 and S.
  • Speed-D is right hinged, the others left hinged.
  • For a single section 48 inches wide or wider, a double door is used (with hinges on left and right).
  • If a EUSERC metering compartment is one of two adjacent sections, that EUSERC section and the other adjacent section will have a double door (the left section, left-hinged; the right section, right hinged).
  • The 36 inch wide Speed-D NEMA 3R enclosure door and the 36 inch wide QED-S/2 door can be interchanged, effecting a "switch" in the side of the section which is hinged;  however, the hinges must be moved (the portions which are bolted to the frame).
  • The part number for a Speed-D 36 in wide NEMA 3R door is 80370-128-50.