Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Why does this Enercept part number have a "s" at the end?

Issue

An Enercept part number (3020EXX-X or 3020BXX-X) has a "s" appended to the end (ex, 3020E08-3S).
Specs for "s" part number are the same for normal part number.
Need to know the difference between appended and normal part number.

Product Line

Enercept meters (part number 3020EXX-X or 3020BXX-X)

Resolution

Enercept part numbers appended with "s" are for sale outside of the US.