Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Are the EX transformer lugs the same part numbers as the EE transformer lugs?

Issue:
Are the EX transformer lugs the same part numbers as the EE transformer lugs?

Product Line:
EX Transformer

Environment:
Digest revision from Digest 176 and Digest 177

Cause:
Clarification

Resolution:
The part numbers for the Lugs have not changed with the new DOE 2106 EX transformers. Part numbers in old 176 Digest are the same used with the new 177 Digest lug listing