Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the maximum weight limit for transformer wall mounting brackets?
Issue:
What is the maximum weight limit of the transformer when using the wall mounting brackets?

Product Line:
Low Voltage Transformers

Environment:
WMB361362, WMB363364, 7400WMB17K, and 7400WMB18K20K

Resolution:
The WMB361362, WMB363364, and 7400WMB17K wall mounting brackets will hold up to a maximum of 700 pounds, but are restricted to Square D/Schneider Electric brand transformers only. These are not designed nor UL listed for other manufacturer's products.

The 7400WMB18K20K wall mounting brackets will hold up to a maximum of 850 pounds, but are restricted to Square D/Schneider Electric transformers only. These are not designed nor UL listed for other manufacturer's transformer products.