Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Do we offer a Twin QMB breaker , or Fusible switch?
Issue:
Does Schneider / Square D offers a Twin QMB breaker, or Fusible switch?

Product Line:
QMB Panel board

Environment:
Application

Cause:
Specification

Resolution:
Yes, but only to certain amperages, ie,Twin Powerpact H frame breaker switches are tandem up to 150A  and twin fusible switches can be ordered as twins at 100A for 240V and 600V switches. A Tandem fusible switch is available for 200A using a QMJ364T, 600V rated switch, with J fuse clips