Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the torque specification for the I-line II busway flanged ends rated 800 - 5000A ?
Issue:
Torque specifications for the I-line II flanged ends rated 800 to 5000A?

Product Line:
AF2330G10FEB and AF2530G10FEB I-Line Busway

Environment:
Products sold in North America

Resolution:
For the FEB type flanged ends, it is 60 - 80 lb-fts for torque values.