Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Does Square D Surgelogic SPDs have communication capabilities?
Issue:
Communication capabilities on SPDs

Product Line:
Surge Protective Device

Environment:
EMA SPD, EBA SPD, HWA, TVS, Surgelogic
ASCO 440, 445, 460,and 465 Series with ASM

Resolution:
Surgelogic SPDs are not capable of communicating via Modbus or Ethernet.  The Surgelogic SPDs use Form C Dry Contacts (24V, 2A) for monitoring the status of the SPD.
ASCO 440 and 460 Series with Active Surge Monitoring (ASM) supports Modbus/TCP, Modbus/RTU, and Ethernet. These units also come equipped with Form C dry contacts (24V, 2A).

Advanced Surge Monitoring (ASM) Product Data
440 Product Data
460 Product Data