Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the inrush for an EX112T212H?
Issue:
Inrush for EX112T212H

Product Line:
Low voltage Transformer

Environment:
Products sold in North America

Resolution:
The inrush of an EX112T212H is 5.8 times the Full Load Amperage (FLA) of the Primary. The Primary FLA (at 208V) is 312A.  312A x 5.8 = an Inrush of 1,809A