Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
5407 Relay output module drops out communication quite frequently.
If the 5407 Relay output module is set to address 0 and the other IO modules, like 5607 IO module is also address 0 the 5407 module respond intermittently or misbehaving.
Solution:
Changed the 5407 module to address 1 or any address that is different from the other IO module address and the problem should be corrected.