Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Is the Model 6 motor control center (MCC) available for a 240V delta system with a high leg?
Issue:
Can you get a MCC rated for a 120/240 3 phase 4 wire high leg system?

Product Line:
Motor Control Center - MCC

Environment:
Model 6

Cause:
Application requirement delta high leg

Resolution:
In Product selectors, the MCC would be entered as 240 v 3Ph 3W. This way the CPT's in the units will be correct. You must put a note in the "Gen Req" tag window- "This is a 240 volt 4 wire with a B-High leg". The plant will then mark this and add a red sign on the MCC about the High Leg. You will need to identify which phase is the high leg. Please be reminded this may impact the delivery code.