Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Video: How to enable/disable Ethernet protocols in ION7400, ION8650, PM8000 and ION9000?

Issue
Configuring Ethernet Protocols and Port Assignments

Product Line
ION9000
PM8000
ION8650
ION7400

Environment
ION Setup 3.0

Resolution

Option 1: In ION Setup, in Setup Assistant, navigate to Communications -> Advanced Ethernet -> Protocols tab. Choose the Protocol that needs to be disabled. Change COMs to Enabled for the the protocol to unchecked.

OPTION1

Option 2: In ION Setup, in Advanced mode, navigate to COMs Modules -> Ethernet -> Setup Registers tab. Choose the Protocol that needs to be disabled. Change the register for the the protocol to No

OPTION 2

Option 3: The PM8000 and ION7400 series meter can enable/disable ethernet protocols through the webserver. Navigate to Setup -> Ethernet -> Advanced Settings. Choose the protocol that needs to be enabled/ disabled. Change the dropdown menu chose to either Yes/ No. Click on Apply to save changes.

OPTION 3