Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Does Sq D offer Panelboards in Nema 3SX?
Issue:
Are Panelboards available in Nema 3SX rating?

Product Line:
NQ/NF/I Line

Environment:
Specification

Cause:
Product Features

Resolution:
The only enclosure rating for NQ /NF / I Line panels , beyond N3R (Not meeting Nema 3SX), is Nema 4X Stainless . The definition of Nema 3SX is below and Nema 4X stainless would meet and exceed Nema 3SX rating as our only offering.
Type 3SX Enclosures constructed for either indoor or outdoor use to provide a degree of protection to personnel against access to hazardous parts; to provide a degree of protection of the equipment inside the enclosure against ingress of solid foreign objects (falling dirt and windblown dust); to provide a degree of protection with respect to harmful effects on the equipment due to the ingress of water (rain, sleet, snow); that provides an additional level of protection against corrosion; and for which the external mechanism(s) remain operable when ice laden.