Issue
What cable can be used to connect the 171CCS7600 to a laptop for programming?
Product Line
Modicon Momentum, ProWORX, Concept, Modsoft.
Resolution
The 171CCS76000 controller has an RJ45 RS232 Modbus port for programming. If you have a DB9 serial port on your Laptop, you can use a combination of a cable and adapter.
What cable can be used to connect the 171CCS7600 to a laptop for programming?
Product Line
Modicon Momentum, ProWORX, Concept, Modsoft.
Resolution
The 171CCS76000 controller has an RJ45 RS232 Modbus port for programming. If you have a DB9 serial port on your Laptop, you can use a combination of a cable and adapter.
Cable - 110XCA28201 (3ft), 110XCA28202 (10ft), 110XCA28203 (20ft).
Adapter - 110XCA20300 - 9pin to RJ45 adapter.
You will need one of the cables + the adapter.
Publicado para: Schneider Electric Mexico