Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Can the BMENOC IP address of a Hot Standby configuration be changed without stopping the process?
Issue
The configured Ip address of the BMENOC needs to be changed without stopping the process.

Product line
Unity Pro, EcoStruxure Control Expert, M580

Resolution
Since Unity Pro V12 there is a block called HSBY_BUILD_OFFLINE that can be used to add DTM devices to an NOC offline without interrupting the process. However, it does not allow the IP Address of the NOC to be changed. In order to change the IP Addresses you will need to stop the process and transfer.

In essence, the only changes that can be done using this block without interrupting are:
1) adding DTM devices, and
2) making logic modifications

No hardware or network configuration changes (including IP Address changes) are allowed.

If the change requires a 'Rebuild All Project', then it is not supported by the HSBY_BUILD_OFFLINE block.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)