Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Why don't I see my M580 firmware version as a selection in Unity?
Issue
While creating a new project or altering an existing one, the actual firmware running in my M580 is not a choice in Unity or Control Expert.

Product line
Unity Pro, EcoStruxure Control Expert, M580

Resolution
Firmware versions are normally not added to Unity Pro if they are strictly released for fixes/enhancements and no new selections are added.

For the Standard controllers, v3.00, v2.60, v2.50, v2.41, v2.30, v2.13, v2.12, v2.01, v1.13 and v1.04 were not added to Unity Pro/Control Expert.
If you were to have a CPU with firmware v2.50 and you did not wish to upgrade it, you can select firmware 2.40 (or lesser) to transfer to the CPU.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)