Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the alternative CT part for current transformer 2NR500L72?
Issue:
What Current transformer can be crossed for a 2NR500L72 CT ?

Product:
Current Transformers

Environment:
Availability

Cause:
Cross Reference

Resolution:
The 2NR500L72 (50:5) doughnut CT Transformer comes with 72" lead length , which is a special. The 2NR500 is the same 50:5 doughnut CT, but wih 24" leads as standard length.