Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the time base for the UNITY-Control Expert PID integral?
Issue
When entering a value for the ti, what is the time base?

Product line
Unity Pro, Control Expert

Resolution
If you are setting the PID Integral with a %MW, then the time base is milliseconds, 1000 = 1 second. Otherwise, if you are simply throwing in a value in a TIME variable, it is a time format such as T#1s, T#500ms etc. (TIME is also ms).