Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Unity Simulator crash
Issue
The simulator crashes within 5 minutes of running with an ACCESSVIOLATION (second chance) by EVT1T error.

Product line
Unity Pro, Control Expert

Resolution
This could be caused by a FreeRunWrapper section which was generated from a legacy conversion but is now 'spurious' code (does not have purpose after conversion).
With this logic, the simulator typically only crashed on Windows 10 and not Windows 7.

The solution is to delete the section as it serves no purpose.