Issue:
When installing breakers in an I Line panel, does anything have be removed , or added to install?
Product Line:
I Line Panelboards
Environment:
Installation
Resolution:
No, there is nothing needed to add breakers to the I Line interior and these are tamper proof bolts that hold the bus stack together. Do not remove these bolts!Removing these bolts will violate any warranty associated with the interior. The interior cannot be reassembled in the field and must be replaced.
Publicado para: Schneider Electric Mexico