Issue:
ATV320 drive so that its in ATV32 identifier mode?
Product Line:
ATV320 series
Environment:
All
Cause:
Wants to use existing CANopen EDS files from the ATV32 on the ATV320 replacement drives.
Resolution:
When using ATV32 EDS file under CANopen in Advantys:
- If the drive ATV320 has version less than version V2.9IE34à the drive used a mechanism with hidden parameter ( AP12), so you can used ATV320 as ATV32 ( Like with Advantys with ATV32 EDS).
- If the drive ATV320 has version equal or greater then version V2.9IE34 --> AP12 is replaced by NTID parameter.
NTID Fieldbus Identifier selection CANopen address is 5F in hex. Its a R/WS address. WS means you can write to the parameter if the drive is stopped.
NTID= 1 Drive will be identified as a ATV32 drive.
NTID= 0 Drive will be identified as a ATV320 drive.
Publicado para: Schneider Electric Mexico