Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Does Ecostruxure control Expert support HVAC library?
Issue:
HVAC library for EcoStruxure Control Expert


Product Line:
Ecostruxure Control Expert


Resolution:
Yes. The HVAC Library function blocks can be used on PLCs of the Quantum, M340 and M580 product family. Ecostruxure Control Expert V15.1 and above is required.

The following are the list of derived function blocks family wise which are available in this release of library.
image1
EcoStruxure Modicon Libraries – HVAC 2022 can be downloaded from the link below
https://www.se.com/ww/en/download/document/MODICONHVAC2022/