Issue:
Needs seismic information and instructions for a SBSAD800R
Product Line:
Sped-D boards
Environment:
SBSAD800R
Cause:
Seismic information
Resolution:
The published information on seismic certification can be found under the attached SPEED-D14 & D15 drawings and its instruction bulletin (80244-812-08 page 13).
Publicado para: Schneider Electric Mexico