Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What does suffix "A" stand for on Cat# RPLHCP32688A?

Product Line:

I-Line Panelboard

Cause:

Need an replacement dead front for a panel. Need to know the difference between deadfront part numbers RPLHCP32688 and RPLHCP32688A.

Resolution:

Argos breakers. It was a change on the deadfront that allowed the J and H breakers to be mounted on the narrow side with access to the advance trip settings without taking off the deadfront. Either the one with the suffix "A" and without it can be used if customer do not need that feature. But some of the Non-A deadfront are not made anymore.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: