Issue
Which programming software can be used for the various Modicon Momentum PLCs?
Product Line
Modicon Momentum
Resolution
There are only 3 active sale Momentum CPUs, 171CBU78090, 171CBU98090 and 171CBU98091. These can only be programmed using Unity Pro / Control Expert.
The rest of the models are Legacy Momentums and were programmed using Concept Programming software if they were IEC/984 or ProWORX if they were strictly 984.
The 171CCC9x020 will only support 984 Ladder Logic programming. The 171CCxx010 and 171CCxx030 will support either IEC or 984LL programming, depending on the executive that is loaded to the M1E.
Publicado para: Schneider Electric Mexico