Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What's the flush mount kit for ASCO 400 series SPD 425120YP10AWAJ10?

Issue:

Replacement for flush mount kit XMFMKITCW for ASCO 400 series SPD 425120YP10AWAJ10

Product Line:

Surge Protection Device

Answer:

Part number for the kit is XMFMKIT. It's the same with the XMFMKITCW.

The CW version was just an identifier showing that it was made in Clearwater, FL, but that facility is closed now so we removed the CW from the part number.