Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Do all the double tub enclosure (MHxxDT20SB) come with knockouts?

Issue:

Does MH50DT20SB have knockouts?

Product Line:

NQ panelboards

Environment:

Products sold in North America

Resolution:

The MHxxDT20SB is two boxes bolted together with one drip hood spanning it. Yes, they have knockouts done.

They all have knockouts as standard. If a blank end wall is needed you would add a BE suffix making it MHxxDT20SBBE.