Issue: SPD breaker protection
Product Line: Surge protection device
Resolution: The SSP04EMA12D is a surge protection device that is certified as UL1449 TYPE 1 device meaning that SPD can be connected to that electrical service directly to that electrical distribution panels bussing without the use of any over current protective device such as a circuit breaker or fuse.
Publicado para: Schneider Electric Mexico