Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
EDCO PC642C / ASCO 175 - How to test to see if Good / Bad
PCB1BWKEY Diagram.JPG


1.  Measure and record the resistance across the following pins on the PCB1BWKEY Plug-in Base (with the EDCO PC642C / ASCO 175 module plugged into the base and all wires disconnected):
> 2-3, 4-5, 6-7, 8-9
2.  If resistance is less than 8 ohms on the EDCO PC642C / ASCO 175 module is good
If resistance is greater than 8 ohms the  EDCO PC642C / ASCO 175 module is bad and should be replaced.

For additional question please reach out to the Schneider Electric SPD Advanced Technical Support Team at 1-800-577-7353.