Issue:
Termination/Lug Wire Sizes
Product Line:
Panelboards
Environment:
I-Line
Cause:
Installation
Resolution:
Main Lug Terminals : (4) 3/0-750 kcmil Al or Cu
(2) Bar A: (34) #4 - 14 AWG AL/CU (Each Bar A = 17 terminations.)
(1) Bar C: (9) #14 - 1/0 AWG AL/CU
(1) Bar D: (7) #6 - 350MCM AL/CU
Publicado para: Schneider Electric Mexico