Product Line:
I-Line Subfeed Lug Kit
Environment:
I-Line Panelboard.
Cause:
Difference between the SL1200P5 and S33930 and it's compatibility with HCR-U I-Line panelboard.
Resolution:
The SL1200P5 will accept (4) 3/0-500 and takes 9" unit mounting space. This subfeed lug kit will work on HCP, HCP-SU and HCRU I-Line interiors.
The S33390 Will accept (4) 3/0-600 and takes 15" unit mounting space. This subfeed lug kit is rated for 800A HCP and HCP-SU max (due to Wire Bending Space) and rated for 1200A in HCRU.
Publicado para: Schneider Electric Mexico