Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
How to wire Current Transformer (CT) on the new HDPM6000S Strip Module (METSEHDPM6S24WF)?
Issue
The redesigned HDPM6000S Strip Module (METSEHDPM6S24WF) doesn’t have the polarity of the CT printed on the Strip Module main circuit board like on the old one. The CT connector (METSEHDPMS24CTCON) doesn’t have polarity printed on it either, but the HDPM6000 CT has two leads White (+) and Black (-). As consequence, landing the connector of the CTs on the Strip Module is concern.

Product Line
HDPM6000 Meter
HDPM6000S
HDPM6000 CT
CT Connectors

Environment
Installation and accessories

Cause
Missing CT polarity printed on the new HDPM6000S Strip Module like on the previous model.

Resolution
While the updated information will be done in the documentation about the correct CT connection on the new HDPM6000S Strip Module (METSEHDPM6S24WF), this article will be used to guide the installer to wire correctly the CTs on the new HDPM6000S Strip Module.
The CT connector never had polarity printed, but it was obvious before to connect the white lead on (+) and the black lead on (-) because the polarity of the CT was printed on the Strip Module Circuit Board of the initial module design. See the pictures below.

Figure 1: CT Connector (METSEHDPMS24CTCON)
CT Connector
Figure 2: HDPM6000S Strip Module (METSEHDPM6S42) old design
Old HDPM6000S Strip Module design

The polarity sign is not available on the connector neither on the new Strip Module. Therefore, it will be updated in the HDPM6000S new Strip Module (METSEHDPM6S24WF) instruction sheet and available to the end users in the coming days. For now, we can refer to the following diagram (Fig. 3) for a detail connection from the CT to the Strip Module.
Figure 3: Temporary connection diagram
Temporary connection diagram

Please see the following links for parts  and documentation for the Head unit, the Strip module, the Current transformer, and the Connector.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto:
  • Documentación de productos
  • Descargas de software
  • Selector de productos
  • Sustitución y reemplazo de productos
  • Centro de ayuda y contacto
  • Encuentra nuestras oficinas
  • Obtén un presupuesto
  • Dónde comprar
  • Comunidad Schneider Electric
  • Empleo
  • Perfil corporativo
  • Informar una conducta indebida
  • Accesibilidad
  • Sala de redacción
  • Inversores
  • EcoStruxure
  • Búsqueda de empleo
  • Blog
  • Política de privacidad
  • Aviso de Cookies
  • Términos y condiciones
  • Change your cookie settings