Issue:
Customers must know the features of their VR Breaker to ensure It will work as required. Moreover, in case repair parts are needed, they should be ordered based on the VR breaker´s features.
Product Line:
MV Switchgear.
Environment:
Metal Clad, VR Circuit Breaker.
Cause:
Maintenance.
Resolution:
In the attached file is pointed out what each digit of the part number/catalog means, these will determine the features of the circuit breaker such as voltages, currents, power supply to trip, and close coils. Please note that this equipment may have up to 5 special features represented by the last 4 or 5 digits.
Customers must know the features of their VR Breaker to ensure It will work as required. Moreover, in case repair parts are needed, they should be ordered based on the VR breaker´s features.
Product Line:
MV Switchgear.
Environment:
Metal Clad, VR Circuit Breaker.
Cause:
Maintenance.
Resolution:
In the attached file is pointed out what each digit of the part number/catalog means, these will determine the features of the circuit breaker such as voltages, currents, power supply to trip, and close coils. Please note that this equipment may have up to 5 special features represented by the last 4 or 5 digits.