Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Is there a SPD for Meter Pak Devices like MPR42200?

Issue:

SPD for Meter Pak Devices like MPR42200

Product Line:

Surge Protection Devices

Answer:

We do not offer any type of surge for Meter Pak Metering devices. There are no provisions in the main bus bars to attach the surge wires. The only option is to install the SPD in the load centers down stream.