Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Can EXN225T239H be used on 240V corner grounded delta?

Issue:

Need to know if a 240v corner grounded delta system will work with a EXN225T239H

240v delta. phase to phase is 240V. phase to ground is 0 volt

Product Line:

Low Voltage Dry Type Transformers

Answer:

The transformer does not care about phase to ground, only phase to phase voltage. The transformer will be 240V phase to phase regardless if corner ground, hi leg or open ground application