Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What does "TA" suffix means in a Powrpact J-frame breaker?

Product Line:

Powerpact H and J-frame circuit breaker

Environment:

LV Circuit Breaker

Cause:

Part number generated on product selector in SE Advantage has "TA" suffix.

Resolution:

The "TA" suffix on a Powerpact H or J-frame breaker part just means that it has English nuts on the OFF end of the breaker instead of lugs. If the customer needs lugs on the OFF end, they can order the breaker without the TA suffix.